Configure DL-SCH Window (Basic LTE-A FDD Downlink)

Before adding a DL-SCH channel as described below, delete the default DL-SCH in the Transport Channel node (or any configured DL-SCH that occupies resource blocks that your new DL-SCH will occupy). If you add a new DL-SCH without deleting a conflicting DL-SCH, a "code conflicted" error appears in the Status Bar and the Status Window when you generate the waveform.

Click the Add Channel button in the Transport Channel node and select DL-SCH or select an existing DL-SCH channel in the Transport channel node and click the Edit Channel Configuration button to open the Configure DL-SCH window.

The following figure shows the Configure DL-SCH window with the default settings after deleting the existing DL-SCH channel shown in Transport Channel. The currently configured DL-SCH is shown in yellow in the resource mapping graph at the bottom of the window.

Subframe Number

Enter the subframe number(s) for the DL-SCH to occupy. You can enter multiple subframes, separated by commas (for example 1,3,5) or a range of subframes (for example 1-5).

Modulation Type

Choices: QPSK |16QAM | 64QAM | 256QAM

Default: QPSK

Select the modulation type for the DL-SCH.

Resource Blocks

Enter the number(s) of the resource block(s) for the DL-SCH to occupy in both slots of the subframe. You can enter multiple resource blocks, separated by commas (for example 1,3,5) or a range of resource blocks (for example 1-5). Your new configuration is displayed in yellow in the resource mapping graph at the bottom of the window.

Click OK to create your configured DL-SCH channel. The software automatically creates the appropriate PDSCH channels in the Physical Channel node.